how can i obtain the file 'imx8.cfg'

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i obtain the file 'imx8.cfg'

1,256件の閲覧回数
jing_xu1
Contributor II

I want to use ubuntu+openocd-0.10.0+JLink to programme on i.MX 8QuadXPlus MEK CPU Board,

I need to use the command 'openocd -f ./openocd/scripts/interface/jlink.cfg -f ./openocd/scripts/target/imx8.cfg' to connect JLink and the board, how can i obtain the file 'imx8.cfg'?

there are only imx21.cfg  imx25.cfg  imx27.cfg  imx28.cfg  imx31.cfg  imx35.cfg  imx51.cfg  imx53.cfg  imx6.cfg imx.cfg in the ./openocd/scripts/target directory.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,169件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

one can download the cfg file from the link in the topic as below:

https://community.nxp.com/message/1070524?commentID=1070524#comment-1070524 

0 件の賞賛
返信