how can i build sof firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i build sof firmware

1,043件の閲覧回数
lenghonglin
Contributor I

Hello, Everyone. i bought imx8mp dev board(not official version) and success run sof.

the default sof version: 

Firmware info: version 1:5:0-cc5ba
 
kernel version: 5.4.70-2.3.0.
 
and i wanna to build the same sof version by myself.
 
at first i build xtensa-imx8m-elf by build tool
 
the i clone sof and `git reset --hard cc5ba`
 
of course, i build successful and get `sof-imx8m.ri`
 
i replace into board  but hang on kernel.
 
lenghonglin_0-1640272264451.png

 

It seem this is a wrong firmware so that dsp cannot load.

 

which step i do wrong, pls tell me , thanks.

0 件の賞賛
返信
1 返信

1,030件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello lenghonglin,

I guess you have to build with extensa toolchain but this work on L5.10.72 BSP.

https://www.nxp.com/docs/en/user-guide/IMX_DSP_USERS_GUIDE.pdf

 

Regards

0 件の賞賛
返信