how can i Download the Freescale i.MX23-EVK BSP??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i Download the Freescale i.MX23-EVK BSP??

1,135 Views
stevenshan
Contributor II

hello,

how can i Download the Freescale i.MX23-EVK BSP??who can help me?

Labels (2)
0 Kudos
Reply
4 Replies

990 Views
stevenshan
Contributor II

Thanks igor,  is  WCE600_10.05.02_SDK.msi  include bsp of I.mx23 EVK ? i  need to install WCE600_10.05.02_SDK.msi,and then bsp will be installed, ringt?

0 Kudos
Reply

990 Views
igorpadykov
NXP Employee
NXP Employee

yes it is for I.mx23 EVK.

~igor

990 Views
igorpadykov
NXP Employee
NXP Employee

Hi steven

i.MX233 Processors|PMU|Freescale

WCE600_10.05.00_SDK : 2010.05 Windows Embedded CE 6.0 Source Code.

Size (K): 23635 Format: zip Rev #: 2010.05 Modified: 6/19/2010


Best regards

igor

990 Views
erikvandenbroek
Contributor I

AFAIK U can use the latest wince600 package. It should contain the iMX233 bsp

U can download it here

i.MX515 Processors|Advanced HMI|Freescale

(Assuming it's the wince60 BSP U are looking for)

0 Kudos
Reply