how can I get the driver of broadreach BCM89810?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can I get the driver of broadreach BCM89810?

1,598 Views
海宁李
Contributor I

Hi there:

    I am now have one i.MX 6Quad SABRE-AI Platform with an Ethernet PHY of BCM89810, and I have bitbaked fsl-image-qt5 , but how can I get the driver of BCM89810?

   I also have a MPC5604EKIT,but dont have the driver of BCM89810 too.

    How can I get it?

Labels (1)
0 Kudos
3 Replies

738 Views
igorpadykov
NXP Employee
NXP Employee

Hi Haining

seems driver is included as part of AVB Stack for IMXAI2ETH-BRC board

Audio Video Bridging Software|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

738 Views
海宁李
Contributor I

Hi :

   I have another question.

    I have finish the yocto project,and bitbake successfully as blow:

       MACHINE=imx6qsabreauto source fsl-setup-release.sh -b build-wayland -e wayland
       bitbake fsl-image-qt5

  after dd cmd ,it boot up successfully from serial display,but the HDMI has no signal.

0 Kudos

738 Views
海宁李
Contributor I

Hi guy

    I have bought the hardware IMXAI2ETH-BRC board from the NXP website, if I want to get the driver,I must pay for it again?

0 Kudos