how I can use pxp in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how I can use pxp in linux

1,872 Views
delauratfrançoi
Contributor II

Hello my name is françois I work with imx7dual sabre board. I use jethro distribution. I want use pxp.

Can I use pxp in user space?

If yes, there exists a library?

if yes have you goat examples.

Thanks for All Help.

Best regards

François

Labels (3)
0 Kudos
Reply
1 Reply

1,195 Views
gary_bisson
Senior Contributor III

Hi François,

If you plan on using GStreamer1.0 I suggest you use the GStreamer-imx plugins which contains some pxp plugins:

GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms

gstreamer-imx/src/pxp at master · Freescale/gstreamer-imx · GitHub

It has been tested and works fine on i.MX7D.

Regards,

Gary

0 Kudos
Reply