hiiiii,what tftlcd is suitable for imx5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hiiiii,what tftlcd is suitable for imx5

1,548件の閲覧回数
vahidnoori
Contributor II

i have a imx5 and imx6 board . i decided to run tft lcd by its. but i dont know what tft is suitable (lvds interface and driver for linux) for this boards???

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,447件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

You can use Freescales 10" LVDS, this is the part number: MCIMX-LVDS1 .

Driver is already in our Linux BSP

1,447件の閲覧回数
vahidnoori
Contributor II

hello.

is each lcd that has LVDS interface supported and matched by imx53?if no

which on of LCD that has LVDS is suitable for imx53?

0 件の賞賛
返信

1,447件の閲覧回数
vahidnoori
Contributor II

is there 4.3" tft lcd that has lvds interface and supported by imx53? in hannstar displays there is 4.3" tft .can it be supported by imx53?

0 件の賞賛
返信