i have a imx5 and imx6 board . i decided to run tft lcd by its. but i dont know what tft is suitable (lvds interface and driver for linux) for this boards???
You can use Freescales 10" LVDS, this is the part number: MCIMX-LVDS1 .
Driver is already in our Linux BSP
hello.
is each lcd that has LVDS interface supported and matched by imx53?if no
which on of LCD that has LVDS is suitable for imx53?
is there 4.3" tft lcd that has lvds interface and supported by imx53? in hannstar displays there is 4.3" tft .can it be supported by imx53?