hiiiii,what tftlcd is suitable for imx5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hiiiii,what tftlcd is suitable for imx5

1,552 Views
vahidnoori
Contributor II

i have a imx5 and imx6 board . i decided to run tft lcd by its. but i dont know what tft is suitable (lvds interface and driver for linux) for this boards???

Labels (2)
Tags (3)
0 Kudos
Reply
3 Replies

1,451 Views
SergioSolis
NXP Employee
NXP Employee

You can use Freescales 10" LVDS, this is the part number: MCIMX-LVDS1 .

Driver is already in our Linux BSP

1,451 Views
vahidnoori
Contributor II

hello.

is each lcd that has LVDS interface supported and matched by imx53?if no

which on of LCD that has LVDS is suitable for imx53?

0 Kudos
Reply

1,451 Views
vahidnoori
Contributor II

is there 4.3" tft lcd that has lvds interface and supported by imx53? in hannstar displays there is 4.3" tft .can it be supported by imx53?

0 Kudos
Reply