hi , Our project USES imx6Q chip, which is equipped with QNX system.The CAN module sends data in a cycle of 20ms, and when the sent data exceeds 50,000 frames, an abnormal termination will occur.The CAN module then stops sending data.

cancel
Showing results for 
Search instead for 
Did you mean: 

hi , Our project USES imx6Q chip, which is equipped with QNX system.The CAN module sends data in a cycle of 20ms, and when the sent data exceeds 50,000 frames, an abnormal termination will occur.The CAN module then stops sending data.

83 Views
Contributor I

 

/* Transmit a CAN message from the specified mailbox */
void can_ringo_tx(CANDEV_RINGO *dev, canmsg_t *txmsg)
{
//fprintf(stderr,"into can_ringo_tx:CANESR = 0x%02x\n",in32(dev->devinfo->base + RINGO_CANESR));
//fprintf(stderr,"***1***\n");
//can_ringo_debug(dev);
//fprintf(stderr,"***2***\n");
CANDEV_RINGO_INFO *devinfo = dev->devinfo;
int mbxid = dev->mbxid;
// Access the data as a uint32_t array
uint32_t *val32 = (uint32_t *)txmsg->cmsg.dat;

/* test by dyb */
volatile uint32_t i;

/*
* IDLE - Idle Status. The IDLE bit indicates, when there is activity
* on the CAN bus
* 1 - The CAN bus is Idle
*
* TX/RX - Transmission/receive status.
* Indicates when the FlexCAN module is transmitting or receiving a message.
* TX/RX has no meaning, when IDLE = 1
* 0 - FlexCAN is receiving when IDLE = 0
* 1 - FlexCAN is transmitting when IDLE = 0
*/
// Wait till bus available
//delay(2000);
//fprintf(stderr,"***3***\n");
#if 0
while((in32(devinfo->base + RINGO_CANESR) & RINGO_CANES_IDLE) == 0);
#endif

#if 1

for (i=0; i<999999;i++)
{
canesr_val = in32(devinfo->base + RINGO_CANESR) & RINGO_CANES_IDLE;
if (canesr_val != 0)
{
break;
}
}
#endif

//fprintf(stderr,"***4***\n");
// Trasmission inactive
devinfo->canmsg[mbxid].canmcf |= ((TRANS_CODE_NOT_READY & 0x0F) << 24);

// Copy message data into transmit mailbox
devinfo->canmsg[mbxid].canmdl = val32[0];
devinfo->canmsg[mbxid].canmdh = val32[1];

if(devinfo->iflags & INFO_FLAGS_ENDIAN_SWAP)
{
// Convert from Little Endian to Big Endian since data is transmitted MSB
ENDIAN_SWAP32(&devinfo->canmsg[mbxid].canmdl);
ENDIAN_SWAP32(&devinfo->canmsg[mbxid].canmdh);
}

/*解决发送CAN ID 不变问题*/
devinfo->canmsg[mbxid].canmid = (txmsg->cmsg.mid & RINGO_CANMID_MASK_EXT) | RINGO_CANMC_FEN;

// Trasmission active 配置添加发送数据len
// devinfo->canmsg[mbxid].canmcf &=0xfff0ffff;

devinfo->canmsg[mbxid].canmcf &=0xffE0ffff;

devinfo->canmsg[mbxid].canmcf |= ((TRANS_CODE_TRANSMIT_ONCE & 0x0F) << 24) | (txmsg->cmsg.len << 16);
//fprintf(stderr,"***6***\n");
}

Labels (1)
0 Kudos
4 Replies

6 Views
Contributor I

Hi  

The imx6Q I use is equipped with QNX system. When receiving data through CAN, the problem of CAN sending will not occur.The can module will stop sending data for a period of time if it is just sending.

0 Kudos

6 Views
NXP TechSupport
NXP TechSupport

linux can driver description can be found in Linux Manual in Linux L4.14.98_2.0.0 Documentation

For qnx issues please apply to qnx tech support.

Best regards
igor

0 Kudos

6 Views
NXP TechSupport
NXP TechSupport

Hi  anbang

qnx is not supported by nxp, issue may be posted on qnx support portal:

foundry27 : Welcome 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

6 Views
Contributor I
  • It should be a CAN driver  problem.Can you provide examples of iMAX6Q CAN drivers.

0 Kudos