help on how to explore the pinpong module APIs to communicate between cores (A9 and M4) with( kernel module to user module) middle ware or applications layer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

help on how to explore the pinpong module APIs to communicate between cores (A9 and M4) with( kernel module to user module) middle ware or applications layer

1,722件の閲覧回数
anilchowdary
Contributor II

Hi All,

need help on how to explore the pinpong module communication between cores (A9 and M4) with middle ware or applications layer.

Known thing is: now communication is happening between cores (A9 and M4) by RPMsg examples (with the imx_pingpong.ko and freeRTOS pingpong application). 

TODO: by using imx_pingpong.ko (A9 side) how we can expose the pinpong module header-files(rpmsg.h) and APIs to middle ware or application layer( or user level) A9 side. please provide any approach or some examples ( kernel module to user module) if you have already done.

Thanks For your valuable support.

Regards

-Anil

ラベル(3)
3 返答(返信)

1,494件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

in case you are looking for exposing RPMSG endpoint to Linux userspace please look at following GitHUB project GitHub - NXPmicro/rpmsg-sysfs: Linux sysfs interface for RPMsg      .

Regards,

PetrL

1,494件の閲覧回数
anilchowdary
Contributor II

Thanks Petr,

the above link will helps a lot. thank you so much.

Regards

-Anil

0 件の賞賛
返信

1,494件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-333803 

hope this document is helpful for you.

0 件の賞賛
返信