heatsink as part of 8MPLUSLPD4-CPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

heatsink as part of 8MPLUSLPD4-CPU

253 次查看
rjm
Contributor IV

Upon delivery of 8Mplus EVK base board, the included SoM 8MPLUSLPD4-CPU comes with a heatsink which is diagonally mounted via two screws.

Of course, this heatsink is not part of the Excel BOM-file, because it's not part of the soldering process.

I don't find a similar heatsink with a diagonal hole distance of 75.4 mm (29.7"). Therefore I'd appreciate it to know manufacturer and order ID.

标记 (1)
0 项奖励
0 回复数