heatsink as part of 8MPLUSLPD4-CPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

heatsink as part of 8MPLUSLPD4-CPU

254件の閲覧回数
rjm
Contributor IV

Upon delivery of 8Mplus EVK base board, the included SoM 8MPLUSLPD4-CPU comes with a heatsink which is diagonally mounted via two screws.

Of course, this heatsink is not part of the Excel BOM-file, because it's not part of the soldering process.

I don't find a similar heatsink with a diagonal hole distance of 75.4 mm (29.7"). Therefore I'd appreciate it to know manufacturer and order ID.

タグ(1)
0 件の賞賛
0 返答(返信)