Hi all,
We have a imx6q platform under yocto (L4.1.15_1.0.0). We used to recording h264 files with it onto sd cards (without gstreamer).
Today, we want to create big record files (>10 Gb). But we observe a limitation of 2 Gb. Even if the recorded sequence is superior to 2Gb, when closing the file, it is truncated at 2 Gb. It's very curious because the sd card is a fat32 one, so at least 4 Gb are expected. It's clearly not our application that is in concern. We suppose it's due to linux system configuration, but where...
Do you have some suggestions about this issue ?
Rgds,
Christophe
Hi Christophe
seems this is limitation of 32-bit systems, issue may be posted on kernel mail list
c - Is O_LARGEFILE needed just to write a large file? - Stack Overflow
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------