gstreamer1.0-plugins-imx building issue with bitbake

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

gstreamer1.0-plugins-imx building issue with bitbake

977 次查看
veeranjaneyulug
Contributor III

Hi Every one,

I'm trying to build bitbake gstreamer1.0-plugins-imx .can you give me instructions,and we got another issue multiple.bb issues also we faced.

error logs mentioned below:

User1@FSETBLR1LX045:~/epdc/yocto/ipcam/fsl-release-bsp/build$ bitbake gstreamer1.0-plugins-imx

Parsing recipes: 100% |########################################################################################################| Time: 00:01:38

Parsing of 1581 .bb files complete (0 cached, 1581 parsed). 2051 targets, 127 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.24.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.7"

TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):f20e4c0cf6ddb29a1aad6e7b095e1472e81d330c"

meta-oe          

meta-multimedia   = "(nobranch):7bbacd0023fa1111da94ba0b2aafd7d872301ffe"

meta-fsl-arm      = "(nobranch):b74e5e690d8d4e149ea9de3f0fcca37bad93935f"

meta-fsl-arm-extra = "(nobranch):b32528c10caac5e85f2b5efe0e5b95322dd68ace"

meta-fsl-demos    = "(nobranch):48cb0bcdd226d2e7eee1fdc222713e1dff93342c"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Command Error: exit status: 126  Output:

/home/User1/epdc/yocto/ipcam/fsl-release-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/quilt: line 153: /home/User1/bin/bash: cannot execute binary file

ERROR: Function failed: patch_do_patch

ERROR: Logfile of failure stored in: /home/User1/epdc/yocto/ipcam/fsl-release-bsp/build/tmp/work/x86_64-linux/gnu-config-native/20120814-r0/temp/log.do_patch.8308

ERROR: Task 230 (virtual:native:/home/User1/epdc/yocto/ipcam/fsl-release-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_20120814.bb, do_patch) failed with exit code '1'

ERROR: Command Error: exit status: 126  Output:

/home/User1/epdc/yocto/ipcam/fsl-release-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/quilt: line 153: /home/User1/bin/bash: cannot execute binary file

ERROR: Function failed: patch_do_patch

ERROR: Logfile of failure stored in: /home/User1/epdc/yocto/ipcam/fsl-release-bsp/build/tmp/work/x86_64-linux/m4-native/1.4.17-r0/temp/log.do_patch.8320

ERROR: Task 894 (/home/User1/epdc/yocto/ipcam/fsl-release-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.17.bb, do_patch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 29 tasks of which 0 didn't need to be rerun and 2 failed.

Waiting for 0 running tasks to finish:

Summary: 2 tasks failed:

  virtual:native:/home/User1/epdc/yocto/ipcam/fsl-release-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_20120814.bb, do_patch

  /home/User1/epdc/yocto/ipcam/fsl-release-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.17.bb, do_patch

标签 (5)
0 项奖励
回复
1 回复

759 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  have you properly setup environment as stated in

“Freescale_Yocto_Project_User's_Guide.pdf”, beginning from section 3 (Host Setup).

What about the machine and distro specifications ?

was minimal system first built ?


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复