gstreamer1.0-plugins-imx build fail on IMX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

gstreamer1.0-plugins-imx build fail on IMX8MP

跳至解决方案
1,094 次查看
shlomz
Contributor III

HI,

when building gstreamer1.0-plugins-imx with yocto (6.1-langdale) it sequently builds libimxvpuapi2 which fails during its configuration stage on:

Checking for library hantro_h1 :
not found

The configuration failed

would appreciate the help.

 

thanks.

标记 (3)
0 项奖励
回复
1 解答
1,073 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please share more details with what steps you've taken and error log. 

Like what DISTRO AND MACHINE you build with? 

I've tried to build with fsl-imx-wayland and imx8mp-lpddr4-evk. Found that some of open sources for this release have been changed. The BSP has been released a bit long. So, can you please use the new BSP and then built it? 

 

Regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,074 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please share more details with what steps you've taken and error log. 

Like what DISTRO AND MACHINE you build with? 

I've tried to build with fsl-imx-wayland and imx8mp-lpddr4-evk. Found that some of open sources for this release have been changed. The BSP has been released a bit long. So, can you please use the new BSP and then built it? 

 

Regards

Harvey

0 项奖励
回复
1,069 次查看
shlomz
Contributor III

im using a custom MACHINE which is basically aligned with imx8mp-lpddr-evk. 

I will try the new BSP and see if it works on imx8mp-lpddr-evk.

as I understand it, gstreamer1.0-plugins-imx should enable freerdp to work with the gstremer libs and thus have hw acceleration on vpu enabled, is it correct?

0 项奖励
回复
1,049 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Is the build working for you with new BSP? 

About the freerdp to work with gstremer libs, please raise a new ticket for further assistance.

 

Regards

Harvey

 

0 项奖励
回复
1,046 次查看
shlomz
Contributor III

yes, but only after updating the src for libimxvpuapi2 to a commit that includes this fix:

https://github.com/Freescale/libimxvpuapi/pull/62/commits/7ad208c83515c34f54200614e3ac6940a9dfb0fa

Otherwise, I get the same linker error during the build.

I suggest NXP updates the recipe

 

thanks!

0 项奖励
回复
1,043 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Thank you, already inform the same to internal team for these updates.

 

Regards

Harvey

0 项奖励
回复