gstreamer plugin for imx are missing in yocto morti ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer plugin for imx are missing in yocto morti ?

2,063 Views
rans
Senior Contributor I

Hello,

We are using yocto morti, which has gstreamer 1.0.

We see that cpu load is 100%

We then found out that probably some plugin are missing:

  • imxipuvideosink :
  • imxg2dvideosink : 
  • imxv4l2videosink 

Does it make sense that they are missing in yocto morti for imx6 ?

How can we add them?

Regards,

Ran

0 Kudos
Reply
1 Reply

1,784 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

imxipuvideosink is part of community gstreamer-imx plugins,

supported by community:

meta-freescale Info Page 

One can try with nxp gstreamer plugins described in attached documents with

nxp bsps on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply