gstreamer - playbin produces "Error parsing H.264 stream" ... "No H.264 NAL unit found"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer - playbin produces "Error parsing H.264 stream" ... "No H.264 NAL unit found"

3,302 Views
adowdy
Contributor II

I have a very simple video stream playing test I'm running on my imx6 hardware that reproduces an unknown parsing issue. Here is the command:

gst-launch-1.0 -v playbin uri="rtsp://192.168.0.123:554/mpeg4?username=admin&password=mypassword"

playbintest1.png

the base plugins that playbin is populating with are from yocto krogoth

OpenEmbedded Layer Index - gstreamer1.0-plugins-base 

OpenEmbedded Layer Index - gstreamer1.0-plugins-good 

OpenEmbedded Layer Index - gstreamer1.0-plugins-imx 

The URI is provided by an H.264 streaming IP camera.

This runs and displays video for a time, but then fails.

ERROR: from element /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstH264Parse:h264parse0: Error parsing H.264 stream
Additional debug info:
../../../gst-plugins-bad-1.6.3/gst/videoparsers/gsth264parse.c(1159): gst_h264_parse_handle_frame (): /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstH264Parse:h264parse0:
No H.264 NAL unit found
Execution ended after 0:08:42.991578062

Why though?

In a comparable test I try to create the simplest pipeline possible manually without playbin and it still uses RtpH264Depay and H264Parse elements like so:

gst-launch-1.0 rtspsrc debug=1 user-id="admin" user-pw="mypassword" location="rtsp://192.168.0.123:554/mpeg4" ! rtph264depay ! h264parse ! imxvpudec ! imxipuvideosink

nonplaybin-pipeline1.png

But this pipeline never produces this error, and can run for days.

Your consideration is appreciated, thank you! - AD

Full log below:

gst-launch-1.0 -v playbin uri="rtsp://192.168.0.123:554/mpeg4?username=admin&password=mypassword"
Setting pipeline to PAUSED ...
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: ring-buffer-max-size = 0
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: buffer-size = -1
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: buffer-duration = -1
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: use-buffering = false
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: download = false
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: uri = rtsp://192.168.0.123:554/mpeg4?username=admin&password=E10ADC3949BA59ABBE56E057F20F883E
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: connection-speed = 0
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: source = "\(GstRTSPSrc\)\ source"
Pipeline is live and does not need PREROLL ...
Progress: (open) Opening Stream
Progress: (connect) Connecting to rtsp://192.168.0.123:554/mpeg4?username=admin&password=E10ADC3949BA59ABBE56E057F20F883E
Progress: (open) Retrieving server options
Progress: (open) Retrieving media info
Progress: (request) SETUP stream 0
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager: latency = 2000
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager: ntp-sync = false
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager: ntp-time-source = NTP time based on realtime clock
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager: drop-on-latency = false
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager: buffer-mode = Slave receiver to sender clock
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc1: timeout = 5000000000
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc1: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\""
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc2: caps = application/x-rtcp
Progress: (open) Opened Stream
Setting pipeline to PLAYING ...
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager: buffer-mode = Slave receiver to sender clock
New clock: GstSystemClock
Progress: (request) Sending PLAY request
Progress: (request) Sending PLAY request
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc1: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc1.GstPad:src: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
Progress: (request) Sent PLAY request
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc1.GstPad:src: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager.GstGhostPad:recv_rtp_sink_0.GstProxyPad:proxypad0: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpSession:rtpsession0.GstPad:recv_rtp_src: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpSession:rtpsession0.GstPad:recv_rtp_sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager.GstGhostPad:recv_rtp_sink_0: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSrc:udpsrc1: timeout = 0
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1\,\ ssrc\=\(uint\)2051050217"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1\,\ ssrc\=\(uint\)2051050217"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0.GstGhostPad:sink.GstProxyPad:proxypad5: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstRtpH264Depay:rtph264depay0.GstPad:src: caps = "video/x-h264\,\ stream-format\=\(string\)byte-stream\,\ alignment\=\(string\)nal"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstRtpH264Depay:rtph264depay0.GstPad:sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstH264Parse:h264parse0.GstPad:sink: caps = "video/x-h264\,\ stream-format\=\(string\)byte-stream\,\ alignment\=\(string\)nal"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstTypeFindElement:typefind.GstPad:src: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstTypeFindElement:typefind.GstPad:sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0.GstGhostPad:sink: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source.GstGhostPad:recv_rtp_src_0_2051050217_96.GstProxyPad:proxypad4: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager.GstGhostPad:recv_rtp_src_0_2051050217_96.GstProxyPad:proxypad3: caps = "application/x-rtp\,\ media\=\(string\)video\,\ payload\=\(int\)96\,\ clock-rate\=\(int\)90000\,\ encoding-name\=\(string\)H264\,\ packetization-mode\=\(string\)1\,\ profile-level-id\=\(string\)640028\,\ sprop-parameter-sets\=\(string\)\"Z2QAKK2EBUViuKxUdCAqKxXFYqOhAVFYrisVHQgKisVxWKjoQFRWK4rFR0ICorFcVio6ECSFITk8nyfk/k/J8nm5s00IEkKQnJ5Pk/J/J+T5PNzZprQCgC3SpAAAAwHgAABDgYEAAJJ8AACky6974XhEI1A\\\=\\\,aO48sA\\\=\\\=\"\,\ config\=\(string\)0000000167640028ad84054562b8ac5474202a2b15c562a3a1015158ae2b151d080a8ac57158a8e84054562b8ac5474202a2b15c562a3a10248521393c9f27e4fe4fc9f279b9b34d081242909c9e4f93f27f27e4f93cdcd9a6b402802dd2a400000301e000004381810000927c0000a4cbaf7be1784423500000000168ee3cb0\,\ a-tool\=\(string\)\"LIVE555\\\ Streaming\\\ Media\\\ v2011.05.25\"\,\ a-type\=\(string\)broadcast\,\ x-qt-text-nam\=\(string\)\"RTSP/RTP\\\ stream\\\ from\\\ Network\\\ Video\\\ Server\"\,\ x-qt-text-inf\=\(string\)mpeg4\,\ x-dimensions\=\(string\)\"\\\ 1280\\\,\\\ 720\"\,\ x-framerate\=\(string\)\"\\\ 15\"\,\ clock-base\=\(uint\)27330564\,\ seqnum-base\=\(uint\)4354\,\ npt-start\=\(guint64\)0\,\ play-speed\=\(double\)1\,\ play-scale\=\(double\)1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstH264Parse:h264parse0.GstPad:src: caps = "video/x-h264\,\ stream-format\=\(string\)byte-stream\,\ alignment\=\(string\)au\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ framerate\=\(fraction\)0/1\,\ parsed\=\(boolean\)true\,\ profile\=\(string\)high\,\ level\=\(string\)4"
[INFO] bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstImxVpuDecoder:imxvpudecoder0.GstPad:sink: caps = "video/x-h264\,\ stream-format\=\(string\)byte-stream\,\ alignment\=\(string\)au\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ framerate\=\(fraction\)0/1\,\ parsed\=\(boolean\)true\,\ profile\=\(string\)high\,\ level\=\(string\)4"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstCapsFilter:capsfilter0.GstPad:src: caps = "video/x-h264\,\ stream-format\=\(string\)byte-stream\,\ alignment\=\(string\)au\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ framerate\=\(fraction\)0/1\,\ parsed\=\(boolean\)true\,\ profile\=\(string\)high\,\ level\=\(string\)4"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstCapsFilter:capsfilter0.GstPad:sink: caps = "video/x-h264\,\ stream-format\=\(string\)byte-stream\,\ alignment\=\(string\)au\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ framerate\=\(fraction\)0/1\,\ parsed\=\(boolean\)true\,\ profile\=\(string\)high\,\ level\=\(string\)4"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstImxVpuDecoder:imxvpudecoder0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstInputSelector:inputselector0.GstSelectorPad:sink_0: always-ok = false
/GstPlayBin:playbin0/GstInputSelector:inputselector0.GstSelectorPad:sink_0: active = true
/GstPlayBin:playbin0/GstInputSelector:inputselector0: active-pad = "\(GstSelectorPad\)\ sink_0"
/GstPlayBin:playbin0/GstInputSelector:inputselector0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink.GstGhostPad:video_sink.GstProxyPad:proxypad8: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstStreamSynchronizer:streamsynchronizer0.GstPad:src_0: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin.GstGhostPad:sink.GstProxyPad:proxypad11: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstQueue:vqueue.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstQueue:vqueue.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstQueue:vqueue.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin.GstGhostPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstStreamSynchronizer:streamsynchronizer0.GstPad:sink_0: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink.GstGhostPad:video_sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstInputSelector:inputselector0.GstSelectorPad:sink_0: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0.GstGhostPad:src_0.GstProxyPad:proxypad7: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0.GstDecodePad:src_0.GstProxyPad:proxypad6: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv/GstVideoConvert:conv.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv/GstVideoScale:scale.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv.GstGhostPad:src: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstImxG2DVideoSink:imxg2dvideosink0.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv.GstGhostPad:src.GstProxyPad:proxypad10: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv/GstVideoScale:scale.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv/GstVideoConvert:conv.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstPlaySink:playsink/GstBin:vbin/GstPlaySinkVideoConvert:vconv.GstGhostPad:sink: caps = "video/x-raw\,\ format\=\(string\)I420\,\ width\=\(int\)1280\,\ height\=\(int\)720\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ chroma-site\=\(string\)mpeg2\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)0/1"
/GstPlayBin:playbin0/GstInputSelector:inputselector0.GstSelectorPad:sink_0: tags = "taglist\,\ video-codec\=\(string\)\"H.264\\\ \\\(High\\\ Profile\\\)\"\;"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpSession:rtpsession0.GstPad:send_rtcp_src: caps = application/x-rtcp
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager.GstGhostPad:send_rtcp_src_0: caps = application/x-rtcp
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstUDPSink:udpsink1.GstPad:sink: caps = application/x-rtcp
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager.GstGhostPad:send_rtcp_src_0.GstProxyPad:proxypad2: caps = application/x-rtcp
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpSsrcDemux:rtpssrcdemux0.GstPad:rtcp_src_2051050217: caps = "application/x-rtcp\,\ ssrc\=\(uint\)2051050217"
/GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstRTSPSrc:source/GstRtpBin:manager/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink_rtcp: caps = "application/x-rtcp\,\ ssrc\=\(uint\)2051050217"


test start 730


ERROR: from element /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstH264Parse:h264parse0: Error parsing H.264 stream
Additional debug info:
../../../gst-plugins-bad-1.6.3/gst/videoparsers/gsth264parse.c(1159): gst_h264_parse_handle_frame (): /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin:decodebin0/GstH264Parse:h264parse0:
No H.264 NAL unit found
Execution ended after 0:08:42.991578062
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...

0 Kudos
Reply
0 Replies