gstreamer definitely broken iMX5X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer definitely broken iMX5X

1,282 Views
hr1z
Contributor I

There is a problem with the gstreamer alsa library.

Excuting the following basic command does not work:

"gst-launch  alsasrc ! alsasink"

 

The above statement works on just about every linux system (pc or embedded).

I've tried different BSP from the Freescale site but I get the same issue.

Fyi, I can play and record audio separately using aplay/arecord.  I suspect there is something with the alsasink module.

Any ideas anyone?

Tags (1)
0 Kudos
Reply
4 Replies

1,045 Views
frostybeard
Contributor I

Assuming you are using Ubuntu...

With the i.mx51, in a previous release I finally got alsasink working in GStreamer by removing pulseaudio. (Google "how to remove pulseaudio") It also helped to add an .asoundrc to my home directory and add this line to it:
pcm.!default plughw:imx3stack
After that Alsa started working.

However, in the latest Efika git release, alsasink works in Gstreamer. I see that pulseaudio and gst-launch use about 30% CPU time when playing audiotestsrc.

0 Kudos
Reply

1,045 Views
mbp
Contributor V

Not sure if this is similar - but it seems like the same core function:

We're trying to route the mic or Audio line in (AUDIO_LIN_L/R on MX51EVK) to the line out (speaker out) or hp out and it does not appear that any combination of the MediaPlayer, AudioManager or MediaRecorder can be exploited to perform this function.  

Any Thoughts or suggestions anyone?

0 Kudos
Reply

1,045 Views
hr1z
Contributor I

Thanks for the reply.

 

I get the same response (msg) as you do. The issue is that it looks like everything is working

but you do not hear any audio. If you execute "gst-launch audiotestsrc ! alsasink" you hear the actual test tone sent to the speaker output. With the previous command you suppose to hear whatever is on the input (mic).

Does your board work when you issue your command?

0 Kudos
Reply

1,045 Views
TimWoodham
Contributor I

on the imx281 evk i get the following response

 

gst-launch  alsasrc ! alsasink

Setting pipeline to PAUSED ...

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstAudioSrcClock

 

what response is returned on the imx51

i'm running 2.6.35

0 Kudos
Reply