Wandboard 3.14.28 kernel
Arch linux,
gstreamer-imx commit 76c15a0e4380f5499a8476685aaede24aac4894c
Merge: 77d81f7 b5a607c
Author: dv1 <dv@pseudoterminal.org>
Date: Thu Aug 11 08:58:37 2016 +0200
I'm having an odd error with gstreamer. I'm streaming an audio/video stream to a file and finding out that the imxv4l2videosrc element has some issues. First of all, the audio is about 2 seconds out of sync with the video. I was able to solve this by inserting a queue into pipeline (see bold below)
gst-launch-1.0 \
flvmux streamable=true name=muxer ! \
filesink location=test.mp4 \
imxv4l2videosrc queue-size=7 fps-n=30 ! queue ! \
imxipuvideotransform ! imxvpuenc_h264 quant-param=31 ! h264parse ! \
muxer.video \
alsasrc ! audio/x-raw,channels=1 ! queue ! \
audioconvert ! \
faac rate-control=2 ! \
muxer.audio
However, that added queue element causes the imxv4l2src to not got into paused state, which blocks gstreamer from closing the stream.
0:00:12.946507050 3886 0xc73c00 INFO GST_STATES gstbin.c:2316:gst_bin_element_set_state:<imxv4l2videosrc0> current PLAYING pending VOID_PENDING, desired next PAUSED <<<----- I NEVER GET PAST HERE WHEN QUEUE ELEMENT IS PRESENT
0:00:12.946672394 3886 0xc73c00 INFO GST_STATES gstelement.c:2372:gst_element_continue_state:<imxv4l2videosrc0> completed state change to PAUSED
0:00:12.946795402 3886 0xc73c00 INFO GST_STATES gstelement.c:2277:_priv_gst_element_state_changed:<imxv4l2videosrc0> notifying about state-cha
nged PLAYING to PAUSED (VOID_PENDING pending)
0:00:12.946975747 3886 0xc73c00 INFO GST_STATES gstbin.c:2807:gst_bin_change_state_func:<pipeline0> child 'imxv4l2videosrc0' changed state to 3(PAUSED) successfully without preroll
Has anyone seen this? I'm also open to a different solution to sync the audio and video that doesn't involve the queue.