gst1.0-fsl-plugin multiple instances of vpuenc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gst1.0-fsl-plugin multiple instances of vpuenc

ソリューションへジャンプ
2,178件の閲覧回数
andrewmurray
Contributor I

I have found a potential issue with the GStreamer 1.0 implementation of vpuenc relating to multiple instances of vpuenc. I have created a very simple gst1.0 command line that reproduces the issue:

gst-launch-1.0 videotestsrc num-buffers=100 ! tee name=d \

        d. ! queue ! vpuenc ! "image/jpeg" ! filesink location=/tmp/file1.jpg \

        d. ! queue ! vpuenc ! "video/x-h264" ! filesink location=/tmp/file1.avi

If I repeatedly run this, 1 in 7 or so runs result in the following:

Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

====== VPUENC: 4.0.2 build on Oct 13 2015 14:35:57. ======

        wrapper: 1.0.57 (VPUWRAPPER_ARM_LINUX Build on Oct  9 2015 12:52:37)

        vpulib: 5.4.27

        firmware: 3.1.1.46061

[INFO]  Product Info: i.MX6Q/D/S

====== VPUENC: 4.0.2 build on Oct 13 2015 14:35:57. ======

        wrapper: 1.0.57 (VPUWRAPPER_ARM_LINUX Build on Oct  9 2015 12:52:37)

        vpulib: 5.4.27

        firmware: 3.1.1.46061

Pipeline is PREROLLING ...

ERROR: from element /GstPipeline:pipeline0/GstVpuEnc:vpuenc1: GStreamer error: negotiation problem.

Additional debug info:

/gstreamer1.0-plugins-base/1.4.1-r0/gst-plugins-base-1.4.1/gst-libs/gst/video/gstvideoencoder.c(1474): gst_video_encoder_chain (): /GstPipeline:pipeline0/GstVpuEnc:vpuenc1:encoder not initialized

ERROR: pipeline doesn't want to preroll.

Setting pipeline to NULL ...

Freeing pipeline ...

Are multiple instances of vpuenc supported? Is there anything I can do to overcome this issue?

Thanks,

Andrew Murray

ラベル(4)
0 件の賞賛
返信
1 解決策
1,803件の閲覧回数
KevinSong
NXP Employee
NXP Employee

Here is the fix. The fix already included in the latest release.

diff --git a/plugins/vpu/gstvpuenc.c b/plugins/vpu/gstvpuenc.c

index 73e7844..e419073 100755

--- a/plugins/vpu/gstvpuenc.c

+++ b/plugins/vpu/gstvpuenc.c

@@ -554,7 +554,7 @@ gst_vpu_enc_set_format (GstVideoEncoder * benc, GstVideoCodecState * state)

                return FALSE;

   }

-       memset(&(enc->open_param), 0, sizeof(VpuEncOpenParam));

+       memset(&(enc->open_param), 0, sizeof(VpuEncOpenParamSimp));

   if (!gst_vpu_enc_decide_output_video_format (benc)) {

                GST_ERROR_OBJECT (enc, "gst_vpu_enc_decide_output_video_format fail.");

                return FALSE;

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,803件の閲覧回数
andrewmurray
Contributor I

I've debugged this and determined that the reason this occurs is due to corruption of the gstvideoencoder.c _GstVideoEncoderPrivate structure. This results in the value of the 'do_caps' member changing which leads to the GST_EVENT_CAPS event not being handled correctly. It seems that the majority of members in this structure become corrupt.

It seems that KevinSong​ has previously seen this issue (see GStreamer-devel - How to debug Gstreamer memory issue? ) and concluded the root cause was 'an invalid memory write in our hardware accelerate video encoder'.

KevinSong​ can you provide details of the fix for this? Is the corruption caused by the gst1.0-fsl-plugins elements or in some of the binary components such as vpulib etc? I'm not using the very latest (fsl 4.0.2 / gst 1.41) and keen to learn which component I may be able to update to resolve this.

Thanks,

Andrew Murray

0 件の賞賛
返信
1,804件の閲覧回数
KevinSong
NXP Employee
NXP Employee

Here is the fix. The fix already included in the latest release.

diff --git a/plugins/vpu/gstvpuenc.c b/plugins/vpu/gstvpuenc.c

index 73e7844..e419073 100755

--- a/plugins/vpu/gstvpuenc.c

+++ b/plugins/vpu/gstvpuenc.c

@@ -554,7 +554,7 @@ gst_vpu_enc_set_format (GstVideoEncoder * benc, GstVideoCodecState * state)

                return FALSE;

   }

-       memset(&(enc->open_param), 0, sizeof(VpuEncOpenParam));

+       memset(&(enc->open_param), 0, sizeof(VpuEncOpenParamSimp));

   if (!gst_vpu_enc_decide_output_video_format (benc)) {

                GST_ERROR_OBJECT (enc, "gst_vpu_enc_decide_output_video_format fail.");

                return FALSE;

0 件の賞賛
返信
1,803件の閲覧回数
andrewmurray
Contributor I

Thanks for the very quick response. This has solved my issue :smileyhappy:.

0 件の賞賛
返信