gst-launch issue with yocto build of i.mx8mmevk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gst-launch issue with yocto build of i.mx8mmevk

ソリューションへジャンプ
4,604件の閲覧回数
jefflfree
Contributor III

gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=1920,height=1080 ! waylandsink

works on the NXP-provided L4.14.90_2.0.0_ga_images_MX8MMEVK/fsl-image-validation-imx-imx8mmevk.sdcard.

pastedImage_4.png

However, if I use Yocto to build the image using:

DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland

bitbake fsl-image-validation-imx

I just get a black screen with the above gst-launch-1.0 command:

pastedImage_3.png

Any advice?

Jeff

ラベル(1)
0 件の賞賛
返信
1 解決策
4,379件の閲覧回数
jefflfree
Contributor III

Problem solved.

gstreamer does not work properly with the this DISTRO.

DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland

 

I have to use:

DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-xwayland

I have seen comments in community.nxp.com where people have said fsl-imx-wayland is ok, but it really depends on what you are trying to do. Just note, I have found gstreamer does NOT work with this. You need to use fsl-imx-xwayland. I don't know the exact root cause (already spend countless hours building different recipes), but hopefully this helps the rest of you.

Jeff

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
4,379件の閲覧回数
jefflfree
Contributor III

I found fsl-image-validation-imx-imx8mmevk.manifest in both the NXP demo folder and my local Yocto build folder and when I compare the two they are quite different. I looked at the file SCR-4.14.98_2.0.0_ga and it lists some patches that were added to the META_FSL_BSP_RELEASE. I am not sure if this is relevant. Of the ones I diffed,  I see the ones related to gstreamer but I am guessing these don't matter.


gstreamer1.0-plugins-base-ximagesink aarch64_mx8mm 1.14.4.imx
gstreamer1.0-plugins-base-xvimagesink aarch64_mx8mm 1.14.4.imx
gstreamer1.0-plugins-good-ximagesrc aarch64_mx8mm 1.14.4.imx

0 件の賞賛
返信
4,379件の閲覧回数
jefflfree
Contributor III

I reran the Yocto flow using Ubuntu 16.04.1 and I now see a very dark image from gst-launch. Any advice for debugging this issue?

0 件の賞賛
返信
4,379件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you try to use demo image first? if still has the same issue, pls tell me what image and dtb file in demo image you use, let me reproduce this on my board,

0 件の賞賛
返信
4,379件の閲覧回数
jefflfree
Contributor III

Thanks for your reply. Which demo image are you referring to?

0 件の賞賛
返信
4,379件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
4,379件の閲覧回数
jefflfree
Contributor III

I had a typo in my original reference to what worked:

The NXP provided image L4.14.98_2.0.0_ga_images_MX8MMEVK/fsl-image-validation-imx-imx8mmevk.sdcard works. But when I try to build using Yocto, it fails.

0 件の賞賛
返信
4,379件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes I know that .sdcard in demo image works, I mean that you can try the demo kenerl image instead of your own built image to test first

0 件の賞賛
返信
4,379件の閲覧回数
jefflfree
Contributor III

Please elaborate the steps as I am relatively new to this process.

0 件の賞賛
返信
4,380件の閲覧回数
jefflfree
Contributor III

Problem solved.

gstreamer does not work properly with the this DISTRO.

DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland

 

I have to use:

DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-xwayland

I have seen comments in community.nxp.com where people have said fsl-imx-wayland is ok, but it really depends on what you are trying to do. Just note, I have found gstreamer does NOT work with this. You need to use fsl-imx-xwayland. I don't know the exact root cause (already spend countless hours building different recipes), but hopefully this helps the rest of you.

Jeff

0 件の賞賛
返信
4,379件の閲覧回数
jefflfree
Contributor III

If you are referring to videotestsrc:

I run this and I get a green screen which is not what it is supposed to do.

gst-launch-1.0 -v videotestsrc ! autovideosink

0 件の賞賛
返信