graphics version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

graphics version

1,173 次查看
erikraynolds
Contributor IV

Documentation says:

The kernel module version of graphics used on the system can be found by running the following command on the board:
dmesg | grep Galcore

I got response:

root@imx6qpsabreauto:~# dmesg | grep Galcore
[ 0.836271] Galcore version 5.0.11.41671

The user-side GPU drivers version of graphics can be displayed using the following command on the board:
grep VERSION /usr/lib/libGAL*

root@imx6qpsabreauto:~# grep VERSION /usr/lib/libGAL*
Binary file /usr/lib/libGAL.so matches

I'm not getting version number: What's the GPU drivers version?

标记 (1)
0 项奖励
回复
2 回复数

1,044 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Erick:

This may help:

https://community.nxp.com/thread/308582 

regards

0 项奖励
回复

1,044 次查看
erikraynolds
Contributor IV

Nope your link did not help. 

0 项奖励
回复