graphics performance of the iMX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

graphics performance of the iMX28

1,031 Views
ernstzberg
Contributor I

Is there any benchmark to show the graphics performance of the iMX28?

0 Kudos
Reply
1 Reply

925 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ernst

I am afraid there are no such benchmarks.

However you can try yourself for example latest demo

Public images - fsl-community-bsp/master/266/x11/imx28evk

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply