gputop: libgpuperfcnt can't be found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

gputop: libgpuperfcnt can't be found

1,739 次查看
vmbtech
Contributor I

Hi there, trying to build gputop and it seems I need libgpuperfcnt

https://source.codeaurora.org/external/imx/imx-gputop/

I see in meta-freescale/SCR/SCR-5.15.5-1.0.0.txt the following references to it, but not sure how I can get a link to download it or if it has any source files which I'm sure I will need

Package:                     libgpuperfcnt-6.4.3.p4.0-aarch64-wayland.bin
Version:                     6.4.3.p4.0
Outgoing License:            LA_OPT_NXP_Software_License v34 February 2022 - Additional distribution license granted - Section 2.3 applies
License File:                COPYING
Package Category:            Graphics
Type of Content:             binary
Description and comments:    Library to retrieve i.MX GPU performance data
Release Location:            Mirror
Origin:                      NXP (proprietary)

--------------------------------------------

Package:                     libgpuperfcnt-6.4.3.p4.0-arm-fb.bin
Version:                     6.4.3.p4.0
Outgoing License:            LA_OPT_NXP_Software_License v34 February 2022 - Additional distribution license granted - Section 2.3 applies
License File:                COPYING
Package Category:            Graphics
Type of Content:             binary
Description and comments:    Library to retrieve i.MX GPU performance data
Release Location:            Mirror
Origin:                      NXP (proprietary)

--------------------------------------------

Package:                     libgpuperfcnt-6.4.3.p4.0-arm-wayland.bin
Version:                     6.4.3.p4.0
Outgoing License:            LA_OPT_NXP_Software_License v34 February 2022 - Additional distribution license granted - Section 2.3 applies
License File:                COPYING
Package Category:            Graphics
Type of Content:             binary
Description and comments:    Library to retrieve i.MX GPU performance data
Release Location:            Mirror
Origin:                      NXP (proprietary)

0 项奖励
回复
2 回复数

1,722 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

gputop and libgpuperfcnt builds for linux BSP seem broken in 5.15 indeed. You have to enter a case (make sure you have nda) to attached to the thread patches for the makefiles so you can build. 

Before running the command, you would need to enable vProfiler option as described in  "12.6.3.1 Enable vProfiler option in kernel" from "i.MX Graphics User's Guide" in order to get proper occupancy values.

Regards

0 项奖励
回复

1,539 次查看
ChristianPrather
Contributor II

Hello, has this been resolved? When attempting to build libgpuperfcnt bb file I get the following fetch error. 


libgpuperfcnt-6.4.3.p4.6-r0 do_fetch: Failed to fetch URL https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.3.p4.6-aarch64-fb.bin;fsl-eula=true;nam..., attempting MIRRORS if available

Seems like there is a missing bin in the lgfiles dir or the link is incorrect. Any assistance would be greatly appreciated.

Related Issue:

https://community.nxp.com/t5/i-MX-Processors/libgpuperfcnt-6-4-3-p1-4-can-t-be-fetched-in-Yocto-Zeus...