Hello,
We are trying to video playback only over iMX28 base customize borolo h/w, This h/w is not supported any audio.
Do you have any suggestions for helping us with these following issues given below & attached. Any help would be appreciated.
we have changed kernel configuration and selected gstreamer/multimedia codecs packages using ltib kernel/menu config and build successfully.
------------------------------------------------------
We have configured for kernel driver in ltib :
Linux Kernel Configuration->
Device Drivers->
Multimedia support ->
Video For Linux
Enable Video For Linux API 1 (DEPRECATED) //but "Enable Video For Linux API compatible layer" this field doesn't exists. ********
Compile Remote Controller keymap modules
Enable IR raw decoder for ... (all of them)
Video capture adapters ->
MXS PxP
------------------------------------------------------
Packages selects for gstreamer/multimedia codecs : ltib menu config Freescale Multimedia Plugins/Codecs -->
[*] gstreamer-fsl-plugins
---gstreamer
[*] gstreamer-plugins-good
------------------------------------------------------
"/dev/video0" node is created successfully.
Under "/usr/lib/gstreamer-0.10/' this folder :: "libmfw_gst_mpeg4aspdec.so" lib is created.
We used .mp4 media format that contains mpeg4 video stream only. We are trying to run gplay/gst-launch/gst-inspect for only video play only, some warning/errors console message, log file is also attached here.
"(gst-inspect-0.10:2326): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mpeg4aspdec.so': lib_MPEG4ASP_dec_arm9_elinux.so.1.2.1: cannot open shared object file: No such file or directory"
If we make this symbolic link manually after that able to run gplay/gst-launch without error/warning message on console but no video playback output on lcd screen(4.3 inch, 7 inch).
With Regards,
Surajit Pal