gplay-1.0 to play a music file and click into back camera,then music can not playing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gplay-1.0 to play a music file and click into back camera,then music can not playing

483件の閲覧回数
wangcao
Contributor II

when i use gplay-1.0 to play a music file, then i click into back camera,gstreamer has a warn:    alsa gstalsasink.c:989:xrun_recovery:<alsasink1> xrun recovery -32: Broken pipe

 why have this error, What is the situation this error produce?  and music can not playing.

i use imx6q board, bsp is fsl-release-bsp-L4.1.15_2.1.0.

ラベル(2)
0 件の賞賛
1 返信

403件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Max

one can test on i.MX6 Sabre SD reference board with Demo Images from link

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛