gplay-1.0 to play a music file and click into back camera,then music can not playing

cancel
Showing results for 
Search instead for 
Did you mean: 

gplay-1.0 to play a music file and click into back camera,then music can not playing

247 Views
wangcao
Contributor II

when i use gplay-1.0 to play a music file, then i click into back camera,gstreamer has a warn:    alsa gstalsasink.c:989:xrun_recovery:<alsasink1> xrun recovery -32: Broken pipe

 why have this error, What is the situation this error produce?  and music can not playing.

i use imx6q board, bsp is fsl-release-bsp-L4.1.15_2.1.0.

Labels (2)
0 Kudos
1 Reply

167 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Max

one can test on i.MX6 Sabre SD reference board with Demo Images from link

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos