gpio signal is not varying?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpio signal is not varying?

793 Views
pooja_todakar
Contributor I

hello,

I am configuring the  CSI_DATA04 pad to GPIO4_IO25 in imx6ull processor board but the gpio signal is not varying  with high and low in command line.what is the issue?how to resolve it?

Labels (1)
0 Kudos
Reply
1 Reply

752 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pooja

it may be hardware problem, one can attach jtag debugger and try to toggle

gpio with jtag.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply