Hi,
my current rootfs setup on an iMX6Q is
- Ubuntu 12.04 armel (without Unity)
- imx_3.0.35_4.0.0 kernel
- Xorg server 1.11.4
- gpu-viv-bin-mx6q-3.0.35-4.0.0.bin
- xserver-xorg-video-imx-viv-3.0.35-4.0.0.tar.gz
I have the Xorg server running without any window manager and when I start the glxgears or the es2gears example app I see just a black rectangle.
Only starting the glxgears with the -fullscreen argument shows the glxgears in a small rectangle on the left bottom of the screen. (so no fullscreen at all ...)
It seems that my problem here is similar to that two posts!?!
Re: gpu libs 4.6.9-p9 with x11 (DRI): full-screen only ?
Black rendering of windowed Open GLES applications on iMX6 Vivante under X11
With the Freescale Ubuntu Oneiric 4.0.0 rootfs the glxgears and es2gears example app works. One difference is that I does not use Unity on my 12.04 precise rootfs.
Any hints to solve this issue are welcome. :smileyhappy:
Cheers
-
Benjamin Federau
解決済! 解決策の投稿を見る。
With the following setup I could get the glxgears/es2gears working on my board.
- imx_3.0.35_4.0.0 kernel with Kernel patches from the Yocto FSL layer
- xserver-xorg-video-imx-viv-3.5.7-1.0.0-alpha.2.tar.gz
- gpu-viv-bin-mx6q-3.5.7-1.0.0-alpha.2-hfp.bin
- rebuild libdrm package with a patch from the Yocto FSL layer
But now I have another issue with these Vivante alpha.2 driver. I have connected a touchscreen with a resolution of 1366x768, but with this resolution I get a displaced X desktop. With a resolution of 1280x800 the X desktop is displayed correctly, but this is the wrong resolution for my display.
To make the 1366x768 available I added to linux-2.6-imx/drivers/video/mxc/ldb.c
static struct fb_videomode ldb_modedb[] = {
....
{
"AUO-G156XW01", 60, 1366, 768, 13255, 104, 32, 20, 6, 64, 12,
0,
FB_VMODE_NONINTERLACED,
0,
}
}
This configuration works with the standard mesa driver/libs, but not with the Vivante alpha.2
Did anybody made some experience with display configuration and Vivante driver?
Edit:
The displaced X output could be solve by changing the resolution in the linux-2.6-imx/drivers/video/mxc/ldb.c from
"AUO-G156XW01", 60, 1366, 768, 13255, 104, 32, 20, 6, 64, 12,
to
"AUO-G156XW01", 60, 1360, 768, 13255, 104, 32, 20, 6, 64, 12,
see Enable 1366x768 LVDS screen on MX53 LVDS 0, Android R10.3.1 -blog archive
Unfortunately X11 is not supported on the Official Release of the i.MX6 BSP. However, there is a comment on one of the threads you mention saying that there is a patch on the fsl-community Yocto BSP so I would recommend looking at it.
As for the official BSP release, the next BSP for i.MX6 is expected to support Wayland.
With the following setup I could get the glxgears/es2gears working on my board.
- imx_3.0.35_4.0.0 kernel with Kernel patches from the Yocto FSL layer
- xserver-xorg-video-imx-viv-3.5.7-1.0.0-alpha.2.tar.gz
- gpu-viv-bin-mx6q-3.5.7-1.0.0-alpha.2-hfp.bin
- rebuild libdrm package with a patch from the Yocto FSL layer
But now I have another issue with these Vivante alpha.2 driver. I have connected a touchscreen with a resolution of 1366x768, but with this resolution I get a displaced X desktop. With a resolution of 1280x800 the X desktop is displayed correctly, but this is the wrong resolution for my display.
To make the 1366x768 available I added to linux-2.6-imx/drivers/video/mxc/ldb.c
static struct fb_videomode ldb_modedb[] = {
....
{
"AUO-G156XW01", 60, 1366, 768, 13255, 104, 32, 20, 6, 64, 12,
0,
FB_VMODE_NONINTERLACED,
0,
}
}
This configuration works with the standard mesa driver/libs, but not with the Vivante alpha.2
Did anybody made some experience with display configuration and Vivante driver?
Edit:
The displaced X output could be solve by changing the resolution in the linux-2.6-imx/drivers/video/mxc/ldb.c from
"AUO-G156XW01", 60, 1366, 768, 13255, 104, 32, 20, 6, 64, 12,
to
"AUO-G156XW01", 60, 1360, 768, 13255, 104, 32, 20, 6, 64, 12,
see Enable 1366x768 LVDS screen on MX53 LVDS 0, Android R10.3.1 -blog archive