glTexDirectVIVMap leads GL_INVALID_ENUM if malloc is used

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

glTexDirectVIVMap leads GL_INVALID_ENUM if malloc is used

2,345件の閲覧回数
valkov
Contributor I

Hi, could somebody explain why glTexDirectVIVMap always leads GL_INVALID_ENUM error in following case?

Tried different formats, sizes, etc.

GLuint physical = ~0U;

void *bits = malloc(vF.width() * vF.height());

glBindTexture(GL_TEXTURE_2D, tmpTexId);

glTexDirectVIVMap(GL_TEXTURE_2D,vF.width(),vF.height(), GL_VIV_YV12, (GLvoid **)&bits, &physical); ASSERT(glGetError() != GL_INVALID_ENUM);

Originally the problem with GL_INVALID_ENUM happened when tried to play video/x-theora video using following pipeline:

filesrc ! oggdemux !  theoradec  !  qtvideorenderersink

Where qtvideorenderersink takes GstBuffer, maps it using gst_video_frame_map, takes data and use glTexDirectVIVMap to map data to texture. 

This pipeline produces GL_INVALID_ENUM and no video playback.

In case if format is video/x-h264,   following pipeline is used:

filesrc ! qtdemux ! h264parse ! imxvpudec ! qtvideorenderersink

Everything works, video is successfully played.

 

So if I change original x-theora pipeline to:

filesrc ! oggdemux ! theoradec ! imxipuvideotransformqtvideorenderersink

glTexDirectVIVMap works correctly without any error and video/x-theora content is shown.

So adding imxipuvideotransform makes some magic.

Does it work because it uses imxipuallocator ?

Or glTexDirectVIVMap does not allow to use CPU (not configured?) memory at all on some circumstances ?

imx6 nitrogen board on yocto.

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,113件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Val,

It is difficult to provide a response about the such error with the complete code, do you think you can provide the init function and the headers that you add, and maybe an screen shot of such error.  what version of BSP are you using?, which device are you handling?

You can check attached document Chapter GPU Memory Introduction for more GPU memory usage.

In theory there is no maximum limitation for GPU memory, but you need leave enough system memory for other apps.

Regards

0 件の賞賛
返信

2,113件の閲覧回数
valkov
Contributor I

Hi, thanks for reply.
Updated the post.

And en sample with malloc and glTexDirectVIVMap I took from i.MX_Graphics_User's_Guide.pdf

0 件の賞賛
返信