Hi All,
I am getting below error while booting imx7 based custom board.
cpu cpu0: failed to get the regulator
imx7d-cpufreq: probe of imx7d-cpufreq failed with error -2
What can be the reason for it?
Am i missing anything in device tree? @
Hi Jagdish,
I am guessing you are not using the PF3000 PMIC?
I had a similar issue which was caused by line 194 in drivers/cpufreq/imx7-cpufreq.c:
arm_reg = devm_regulator_get(cpu_dev, "arm");
which is looking for the regulator "arm-supply" under the cpu parent of the device tree.
If, as in my case, it is not convenient to place the supply under the cpu parent, you can try making the following change to line 194:
- arm_reg = devm_regulator_get(cpu_dev, "arm");
+ arm_reg = devm_regulator_get(&pdev->dev, "arm");
linux-2.6-imx.git - Freescale i.MX Linux Tree
Jacob
Hi jagdish
one can check presence &cpu0 { arm-supply = <&sw1a_reg>
as in imx7d-sdb.dts example
linux-2.6-imx.git - Freescale i.MX Linux Tree
One can try to debug it more using attached Linux Manual
Chapter 23 CPU Frequency Scaling (CPUFREQ) Driver
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igorpadycov,
Thanks for your reply.
&cpu0 { arm-supply = <&sw1a_reg> is already available in device tree by default. but still i am getting this error. i have gone through respective section of the document you have attached, but it didn't help me to resolve this issue.
Is it anything related to PMIC?
"sw1a_reg" is available in PMIC phandle in device tree. Currently i am facing some issue with PMIC? Can it be the reason?