continue this problem how do i solve this problem relocation 28 out of range i.mx6
Gcc build kernel in -O0, module's cflag use -O1
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
[ 0.000000] lowmem : 0x80000000 - 0xc0000000 (1024 MB)
[ 0.000000] pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
[ 0.000000] modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
[ 0.000000] .text : 0x80008000 - 0x81b47e38 (27904 kB)
[ 0.000000] .init : 0x81b48000 - 0x81c2f6c0 ( 926 kB)
[ 0.000000] .data : 0x81c30000 - 0x81cc75e0 ( 606 kB)
[ 0.000000] .bss : 0x81cc75e0 - 0x81d865fc ( 765 kB)
.
.
.
[ 14.173801] compat: section 2 reloc 4 sym 'genl_unregister_family': relocation 28 out of range (0x7f0000b8 -> 0x811414e4)
.text part become larger
how do i solve this problem => relocation 28 out of range
I TRY add KBUILD_CFLAGS cflag -mlong-calls still failed....
how to rearrange code~~~?
my compat section in the /hardware not under the /kernel_imx
modify vmlinux.lds.S ???
or
modify the directory to build code on another place like kernel_imx/drivers?
here are some info but not solve problem
1. far_away_symbol
Mailing List Archive: Re: ARM: relocation out of range (when loading a module)
2. modify vmlinux.lds.S
Mailing List Archive: Re: ARM: relocation out of range (when loading a module)
3.mlong-calls
[PATCH] ARM: MMUless Core: Fix insmod error - module relocation out of range
I had this issue on an imx7 project and found the solution was adding the -mlong-calls. Both the kernel modules and the zImage had to be rebuilt with the flag before the relocation error disappeared in the kernel output.
Hi jesse
to overcome branch size limit one can try to create additional
branch table or try various compiler optimization options.
Also since this is specific compiler problem recommended to post
it to gcc mailing list
GCC mailing lists- GNU Project - Free Software Foundation (FSF)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
already use -mlong-calls but failed again
create additionalbranch table
how to do????????? need help
For obtaining full solution for custom task one can apply to NXP Professional Services:
http://www.nxp.com/pages/freescale-professional-services:PROFESSIONAL-SERVICES
Best regards
igor
But I still want to have all kernel compile with -O0 -g
its more easier to use kgdb or openocd to debug struct and value
If someday freescale have new compiler to support -mlong-calls
and do branch long jump is no problem please me know
still need a good gcc compiler for branch long jump
i want to debug driver so i use this way to solve
gedit free_imx/myandroid/kernel_imx/Makefile
KBUILD_CFLAGS += -O2 -g
gedit free_imx/myandroid/kernel_imx/drivers/Makefile 
add in first line
| KBUILD_CFLAGS | += -O0 -g |