gcc-4.6.2 on I.mx28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gcc-4.6.2 on I.mx28

762 Views
jeanletutour
Contributor II

For some application gcc-4.4.4 is no more sufficient

does somebody knows how  to get this compiler gcc-4.6.2,  working for I.mx28 ?

can we compile only the application without recompiling the kernel,  and libs  ?

Thanks

Labels (2)
0 Kudos
2 Replies

607 Views
b36401
NXP Employee
NXP Employee

Actually it does not matter which compiler is used to compile your binaries.

However you need to make sure that you are using right libc.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

607 Views
jeanletutour
Contributor II

Hi Victor , and thanks for your answer , so any version of compiler may work , if you have the good libc .

does  somebody knows  where to get gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm that seems to  be the right version mentionned  in LTIB 

best regards

0 Kudos