games are not playing well

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

games are not playing well

1,008 Views
hariprasathgopa
Contributor II

Hi,all

I use a custom board similar to sabresd. And bsp is android kitkat. When I run games and have follow error, and don’t running success:

E/Unity   ( 3230): findConfigAttrib (30e1): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e1): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e2): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e2): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (3147): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (3147): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e1): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e1): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e2): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e2): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (3147): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (3147): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e1): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e1): EGL error: 0x3004

E/Unity   ( 3230): findConfigAttrib (30e2): EGL error: 0x3004

whether my GPU is enable, if so how to check the usage of GPU

Why? And how to resolved?

Thanks

Hari

Labels (4)
0 Kudos
Reply
1 Reply

868 Views
SergioSolis
NXP Employee
NXP Employee

I did a quick search in the internet and found someone that had the same problem that you have:

http://forum.unity3d.com/threads/angry-bots-example-crash-on-start.127199/

Not sure if it would apply to your problem in the same way, are you able to try it?

0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----