galcore crash with qt application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

galcore crash with qt application

3,804件の閲覧回数
mdilger
Contributor II

Hello,

we are running a linux system build with buildroot on an imx6 dual lite. We use qt webkit application as the front end.

Currently we have an issue with /dev/galcore. The qt application freezes after some period of time, sometimes it happens after 30 minutes, sometimes it takes a whole day or longer for the freeze to occur.

The qt application displays a web page which in case of the error does refresh a clock using java script and communicate with the main application using a web socket and http web service.

The kernel messages show a crash of the driver being stuck

Jan 29 17:44:44 fsimx6 user.warn kernel:   DMA appears to be stuck at this address:
Jan 29 17:44:44 fsimx6 user.warn kernel:     0xFFFA8018

After that error happens the system has to be rebooted to get it working again.

Do you know similar problems or a way to debug it?

Please see the complete output of the crash in the attachment.

ラベル(3)
4 返答(返信)

3,457件の閲覧回数
jiujinhong
Contributor IV

Hi,

Have you fixed this issue? We meet the same issue.

0 件の賞賛
返信

3,457件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Maik,

You can check if it is caused by GPU supply. Also one can try different gpu mem settings, recommended to have 128M gpumem, with 1G system memory, We can not reproduced since you are using build root, try to run in the BSP and see what happens.

Regards

0 件の賞賛
返信

3,457件の閲覧回数
mdilger
Contributor II

Hi,

Also one can try different gpu mem settings, recommended to have 128M gpumem,

Can you tell me how to change the settings then i will look for it. The system memory cannot be changed because it's a COM we get from F&S, we only have these hardware configuration available.

The module is efusA9 COM

Best regards

0 件の賞賛
返信

3,457件の閲覧回数
JohnKaye
Contributor II

Maik,

Did you ever resolve this issue?

Thanks,

-John

0 件の賞賛
返信