[galcore]: GPU[1] hang, automatic recovery.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[galcore]: GPU[1] hang, automatic recovery.

1,954件の閲覧回数
luzhouyang
Contributor I

Core :IMX6QP   when i run screen ,result is this below

can you tell me why ?

**************************
***   GPU STATE DUMP   ***
**************************
  axi      = 0x00000084
  idle     = 0x7FFFFFFE
    FE not idle
  DMA appears to be stuck at this address:
    0x7B805048
  dmaLow   = 0x00000000
  dmaHigh  = 0x00000000
  dmaState = 0x00000000
    command state       = 0 (PAR_IDLE_ST)
    command DMA state   = 0 (CMD_IDLE_ST)
    command fetch state = 0 (FET_IDLE_ST)
    DMA request state   = 0 (REQ_IDLE_ST)
    cal state           = 0 (CAL_IDLE_ST)
    VE request state    = 0 (VER_IDLE_ST)
  Debug registers of pipe[0]:
    RA debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    TX debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    FE debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    PE debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0xA40004F1
      [0x05] 0xABC54001
      [0x06] 0xBC000086
      [0x07] 0xCDE80040
      [0x08] 0xD0000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0xBABEF00D
      [0x0D] 0xBABEF00D
      [0x0E] 0xBABEF00D
      [0x0F] 0xBABEF00D
      signature = 0xBABEF00D (1 read attempt(s))
    DE debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    SH debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    PA debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    SE debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0x00000000
      [0x04] 0x00000000
      [0x05] 0x00000000
      [0x06] 0x00000000
      [0x07] 0x00000000
      [0x08] 0x00000000
      [0x09] 0x00000000
      [0x0A] 0x00000000
      [0x0B] 0x00000000
      [0x0C] 0x00000000
      [0x0D] 0x00000000
      [0x0E] 0x00000000
      [0x0F] 0x00000000
      failed to obtain the signature (read 0x00000000).
    MC debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x0000111C
      [0x03] 0x00000000
      [0x04] 0x12345678
      [0x05] 0x12345678
      [0x06] 0x12345678
      [0x07] 0x12345678
      [0x08] 0x12345678
      [0x09] 0x12345678
      [0x0A] 0x12345678
      [0x0B] 0x12345678
      [0x0C] 0x12345678
      [0x0D] 0x12345678
      [0x0E] 0x12345678
      [0x0F] 0x12345678
      signature = 0x12345678 (1 read attempt(s))
    HI debug registers:
      [0x00] 0x00000000
      [0x01] 0x00000000
      [0x02] 0x00000000
      [0x03] 0xAAAAAAAA
      [0x04] 0xAAAAAAAA
      [0x05] 0xAAAAAAAA
      [0x06] 0xAAAAAAAA
      [0x07] 0xAAAAAAAA
      [0x08] 0xAAAAAAAA
      [0x09] 0xAAAAAAAA
      [0x0A] 0xAAAAAAAA
      [0x0B] 0xAAAAAAAA
      [0x0C] 0xAAAAAAAA
      [0x0D] 0xAAAAAAAA
      [0x0E] 0xAAAAAAAA
      [0x0F] 0xAAAAAAAA
      signature = 0xAAAAAAAA (1 read attempt(s))
    Other Registers:
      [0x0040] 0x00000069
      [0x0044] 0x00000000
      [0x004C] 0x00000000
      [0x0050] 0x00000000
      [0x0054] 0x00000000
      [0x0058] 0x00000069
      [0x005C] 0x0000005F
      [0x0060] 0x0000005F
      [0x043C] 0x00000000
      [0x0440] 0x00000000
      [0x0444] 0x00000000
      [0x0414] 0x3C000000
[galcore]: GPU[1] hang, automatic recovery.

ラベル(1)
0 件の賞賛
返信
1 返信

1,708件の閲覧回数
b36401
NXP Employee
NXP Employee

Please check the processor temperature. Possibly its overheating may cause hanging of its components.

Also please check if the processor is powered fine. I mean the voltage levels is OK and there is no noise.

Also please make sure that you are running the latest BSP. Here may be some updates for GPU driver applied.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信