g2d conversion for RGB24 to RGB565

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

g2d conversion for RGB24 to RGB565

1,934 次查看
saurabh206
Senior Contributor III

Hi

Does g2d is able to do color space conversion between RGB24 to RGB565?

Also does g2d is used to do re-size RGB24 to RGB24?

Thanks

Saurabh

标记 (2)
0 项奖励
回复
2 回复数

1,566 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

I am afraid not, as suggests description in attached

Graphics Guide sect.2.4.1 Color space conversion from YUV to RGB

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,566 次查看
saurabh206
Senior Contributor III

Hi igor,

Thanks for reply.

What is a significance of 2.2.7

pastedImage_0.png

Is there any alternate method to do RGB to RGB scaling other than IPU?

Thanks,

Saurabh

0 项奖励
回复