g2d_blit_2d: fail with status -20

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

g2d_blit_2d: fail with status -20

2,292 次查看
yongtang
Contributor I

Hi,FreeScale

     I meet a very strange question on blit image which with G2D_I420,I blit image with physical continued memory as below,if the source image with 576*360,blit success,but if with 480*300,blit failed,how can i fix this?

     int width = 480;

   int height = 300;

   int o_width = 320;

   int o_height = 240;

  g2d_buf* mpInputBuf = g2d_alloc(width * height * 3 / 2, 0);

  g2d_buf* mpOutputBuf = g2d_alloc(o_width * o_height * 4, 0);

   mInputSurface.planes[0] = mpInputBuf->buf_paddr;

   mInputSurface.planes[1] = mpInputBuf->buf_paddr+ a_width*height;

   mInputSurface.planes[2] = mInputSurface.planes[1] + a_width*height / 4;

   mInputSurface.left = 0;

   mInputSurface.top = 0;

   mInputSurface.right = width;

   mInputSurface.bottom = height;

   mInputSurface.stride = width;

   mInputSurface.width  = width;

   mInputSurface.height = height;

   mInputSurface.rot    = G2D_ROTATION_0;

   mInputSurface.format = G2D_I420;

   mInputSurface.blendfunc = G2D_ZERO;

   mInputSurface.global_alpha = 0;     //Global alpha value 0~255

   mInputSurface.clrcolor = 0;

   mOutputSurface.planes[0] = mpOutputBuf->buf_paddr;

   mOutputSurface.left = 0;

   mOutputSurface.top = 0;

   mOutputSurface.right = o_width;

   mOutputSurface.bottom = o_height;

   mOutputSurface.stride = o_width;

   mOutputSurface.width  = o_width;

   mOutputSurface.height = o_height;

   mOutputSurface.rot    = G2D_ROTATION_0;

   mOutputSurface.format = G2D_RGBA8888;

   mOutputSurface.blendfunc = G2D_SRC_ALPHA;//G2D_ZERO;

   mOutputSurface.global_alpha = 0;     //Global alpha value 0~255

   mOutputSurface.clrcolor = 0;

   if(0 != g2d_make_current(mhG2d, G2D_HARDWARE_2D))

   {    

      return -4;

   }

   g2d_enable(mhG2d,G2D_BLEND);

   if(0 != g2d_blit(mhG2d, &mInputSurface, &mOutputSurface))

   {

      g2d_finish(mhG2d);

    

      return -5;

   }

   g2d_disable(mhG2d, G2D_BLEND);

   if(0 != g2d_finish(mhG2d))

   {    

      return -6;

   }

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,116 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yong

recommended to try latest Vivante v5.0.11p7.4 gpu library (included

in L3.14.52), attached document Table 9. New features shows its

improvements.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复