Hello,
I am working on a imx6 dual custom board based on sabreauto. I have linux-imx 4.1.15 on it. When I try to modprobe the g_ncm driver , if fails to load
Error log is as follows :
g_ncm ci_hdrc.0: failed to start g_ncm: -2
modprobe: ERROR: could not insert 'g_ncm': Unknown symbol in module, or unknown parameter (see dmesg)
And Dmesg shows only one line as
g_ncm ci_hdrc.0: failed to start g_ncm: -2
What can be the possible issue with g_ncm driver. Do we need to provide any module parameters??
-Thanks
Sharvari Harisangam
all modules used cmd “modprobe“
hello,
i have the same question with you,
Do you have get it?
thank you