fw_printenv works after typing in u-boot at least once saveenv

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fw_printenv works after typing in u-boot at least once saveenv

901 Views
mariusoctavian
Contributor IV

I Have a dart Imx8mmq mini from varisicte.

I run kernel: 5.15.60-imx8mm
I build all linux using buildroot
I use Vari debian repos to build u-boot + atf  from sources.
                                                      See below the u-boot details

After I flash the emmc and the board boots up and we acquire the shell the
fw_printenv prints:

Cannot read environment, using default
Cannot read default environment from file


If at least once, after fresh flashing I stop at u-boot prompt and I type saveenv then the fw_printenv and fw_saveenv starts working fine and conserves the env between power cycles

Here is the fw_emv.config

/dev/mmcblk2            0x400000        0x1000

How can I automatically make u-boot to saveenv or after flashing using uuu to make the u-boot to call at least once 'saveenv'

I found a link but targets a u-boot from 2014 and is not longer applicable.

 

Our u-boot excerpt:

Authenticate image from DDR location 0x401fcdc0...


U-Boot 2020.04 (Sep 22 2023 - 12:34:31 -0400)

CPU:   i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Model: Variscite DART-MX8M-MINI
DRAM:  2 GiB
MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from EXT4... Loading Environment from MMC... OK

 

 

Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

870 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @mariusoctavian !

Thank you for contacting NXP Support!

That is not a normal behavior of the U-boot terminal.

Unfortunately you are using a BSP that is not provided by NXP.

I recommend to contacting varisicte to obtain support or refer to the U-boot documentation.

https://u-boot.readthedocs.io/en/latest/


Best Regards!
Chavira

0 Kudos
Reply