fsl,legacy-bch-geometry was removed in kernel 5.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl,legacy-bch-geometry was removed in kernel 5.4

1,096件の閲覧回数
mohamed-ali_fod
Contributor I

Hello,

The device tree property fsl,legacy-bch-geometry which was available in kernel 4.19 is no more present in kernel 5.4, could you please explain how to handle the legacy bch geometry in this case? because in kernel 5.4 the rootfs cannot be mounted form nand flash due to the following error: ubi0 error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB

Note: fsl,legacy-bch-geometry was the solution to fix ubi_io error in 4.19 kernel, below is the thread for reference:

https://community.nxp.com/t5/i-MX-Processors/IMX6-ubi0-attaching-fail-Kernel-4-19-35-uboot-2014-07/m...

Best Regards,

Mohamed Ali

0 件の賞賛
返信
2 返答(返信)

1,085件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

1,031件の閲覧回数
mohamed-ali_fod
Contributor I

Hi Igor,

I am aware about mentioned fix for 4.19 kernel but I am looking for fix of the 5.4 kernel?

Thanks,

Mohamed Ali

0 件の賞賛
返信