fsl-community-bsp daisy branch with image fsl-image-gui

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fsl-community-bsp daisy branch with image fsl-image-gui

2,506 次查看
zhencongtee
Contributor III

Hi,

I am trying to build the daisy or master branch for the Wandboard Solo board. I manage to build the fsl-image-gui image using Dora branch with a nice x11 GUI.

However, i am not able to locate the fsl-image-gui anymore starting Daisy branch. Is the fsl-image-gui image build has been taken out in the Daisy branch?

I needed an image with 3.10.17 kernel + x11 GUI. Any idea which image i should use? The Dora branch kernel version is 3.0.35.

Thank you.

Regards,

Zhen Cong Tee

3 回复数

1,660 次查看
justin_jiang
NXP Employee
NXP Employee

You can find the dora-3.10.17-1.0.0_ga release from Freescale.

And you can use below command to build for x11 GUI:

MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 -e x11

bitbake fsl-image-x11

1,660 次查看
zhencongtee
Contributor III

Hi Jiang,

Thanks for reply.

Can this image be used in the Wandboard? Is there any peripheral differents on the Wandboard and the Freescale SabreSD?

As far as i know, the fsl-image-x11 image is meant for the Freescale SabreSD board.

Regards,

Zhen Cong Tee

0 项奖励
回复

1,660 次查看
justin_jiang
NXP Employee
NXP Employee

I don't know about the Wandboard board. What's it?