fsl-arm-yocto-bsp-imx-4.1-krogoth

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl-arm-yocto-bsp-imx-4.1-krogoth

1,694 Views
末班车上的乘客
Contributor II

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.1.0.xml
fatal: Cannot get https://gerrit.googlesource.com/git-repo/clone.bundle
fatal: error [Errno -3] Temporary failure in name resolution

from china

Labels (2)
0 Kudos
Reply
1 Reply

1,216 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello  贾继中 贾继中 ,

I would recommend checking that you have the repo utility installed. You can install it with the commands on the following link:

FSL Community BSP 

I would also recommend making sure that you have internet access. It's common to have problems when under a firewall or trough a proxy so please review that you can reach git repositories.

I hope this helps!

Regards,

0 Kudos
Reply