fsl-L3.10.53_1.1.0_iMX6qdls_Bundle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl-L3.10.53_1.1.0_iMX6qdls_Bundle

840 Views
1990rahulreddy
Contributor IV

I have dumped fsl-image-qt5-x11-imx6qdlsolo.sdcard on I.MX6 SABRESDB & I can access the terminal using minicorm. How can start writing program in python & execute it. I have to make image processing application on it. How to install OpenCV library in this. Do I need to copy paste file from USB to SD Card...or any simple way of doing this...

Please, give step by step...answer...I am windows user...& new to both i.MX6 & openCV

Labels (2)
0 Kudos
2 Replies

576 Views
igorpadykov
NXP Employee
NXP Employee

HI Rahul

please look at

Computer Vision on i.MX Processors: Building OpenCV-2.4.X for Freescale's i.MX6 BSP (Yocto)

https://community.freescale.com/docs/DOC-95396

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

576 Views
1990rahulreddy
Contributor IV

Computer Vision on i.MX Processors: Building OpenCV-2.4.X for Freescale's i.MX6 BSP (Yocto)

=> For this they explain the to change using bitbake core-image-x11, I have use .sdcard image....how to edit this using bitbake

Building OpenCV on ubuntu hardfloat rootfs for i.MX6Q

=> For this, kernel is different.

Please, let mi know the installation for above kernel

0 Kudos