format of SD card for flashing Android OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

format of SD card for flashing Android OS

Jump to solution
1,145 Views
Ruban1
Contributor II
which Format is recommended for SD card before creating partition and flashing Android OS. because in pdf its mention SD card should be unmount before flashing . So can you suggest me ,Should i format in FAT32 or NTFS format.
0 Kudos
Reply
1 Solution
1,142 Views
b36401
NXP Employee
NXP Employee

Actually it is never mind how the card is formatted. The format will be lost after re-partitioning of the card.

View solution in original post

0 Kudos
Reply
1 Reply
1,143 Views
b36401
NXP Employee
NXP Employee

Actually it is never mind how the card is formatted. The format will be lost after re-partitioning of the card.

0 Kudos
Reply