forcing a first time boot on Android for the iMX51 EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

forcing a first time boot on Android for the iMX51 EVK

878件の閲覧回数
RafaelG_Lopez
Contributor I
Can anyone help me figure out how to force an iMX51 EVK to do a first time boot on Android R8?

I need to do touch screen calibration again.

Thank you.
タグ(1)
0 件の賞賛
3 返答(返信)

731件の閲覧回数
Jackrun2000
Contributor I
My andorid-r8 worked normally. I guess there is something wrong in your compilation. If you want to use android-r8, you must use linux kernel-2.6.31 and compile it with Freescal compiler. I used kernel-2.6.28 for android-r8 and got the same error like you met. Rafael G. Lopez said:
Jack:

Thank you. It works.
I also received this tip from the technical contact at Freescale.
However, after removing the calibration file, it did go through touch screen calibration, but then something else got wrecked, since Android would get stuck during loading, and it did not get to the main screen.

I had to erase the SD card and do a clean installation, which did go through touchscreen calibration.

I guess these are the growing pains of working with the iMX51 for the first time, along with Android, and the touchscreen feature. Too many new things at the same time.

Rafael Lopez

jack kang said:
First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.
0 件の賞賛

731件の閲覧回数
RafaelG_Lopez
Contributor I
Jack: Thank you. It works. I also received this tip from the technical contact at Freescale. However, after removing the calibration file, it did go through touch screen calibration, but then something else got wrecked, since Android would get stuck during loading, and it did not get to the main screen. I had to erase the SD card and do a clean installation, which did go through touchscreen calibration. I guess these are the growing pains of working with the iMX51 for the first time, along with Android, and the touchscreen feature. Too many new things at the same time. Rafael Lopez jack kang said:
First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.
0 件の賞賛

731件の閲覧回数
Jackrun2000
Contributor I
First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.
0 件の賞賛