Dear all,
I have a question about Boot constitution pin of i.MX6.
The BOOT_CFG3[2] selects a frequency for ARM and DDR until Boot loader in the Boot device is executed.
0 - ARM - 792 MHz, DDR - 396 MHz, AXI - 264 MHz
1 - ARM - 396 MHz, DDR - 352 MHz, AXI - 176 MHz
I understand that after Boot Loader was executed, they(ARM/DDR/AXI) work in a setting value in Boot Loader.
(all PLL is set again by Boot Loader.)
Is my understanding right?
Best Regards,
Yuuki