for kogroth with new qt5imageformats getting error like Internal Compiler error, any one faced this issue before?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

for kogroth with new qt5imageformats getting error like Internal Compiler error, any one faced this issue before?

1,018件の閲覧回数
vijaymane
Contributor I

compiling /home/htsl/hon-fusion-bsp/build/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/qtimageformats/5.6.2+gitAUTOINC+d7bdc138b8-r0/git/src/3rdparty/libwebp/src/dsp/upsampling_neon.c
*** stack smashing detected ***: /home/htsl/hon-fusion-bsp/build/tmp/sysroots/i686-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/cc1 terminated
In file included from /home/htsl/hon-fusion-bsp/build/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/qtimageformats/5.6.2+gitAUTOINC+d7bdc138b8-r0/git/src/3rdparty/libwebp/src/dsp/upsampling_neon.c:20:0:
/home/htsl/hon-fusion-bsp/build/tmp/sysroots/i686-linux/usr/lib/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/include/arm_neon.h: In function 'UpsampleRgbaLinePair':
/home/htsl/hon-fusion-bsp/build/tmp/sysroots/i686-linux/usr/lib/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/include/arm_neon.h:6697:10: internal compiler error: Aborted
return (int32x4_t)__builtin_neon_vmlals_lanev4hi (__a, __b, __c, __d);
^
Please submit a full bug report,

0 件の賞賛
返信
1 返信

844件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Vijay,

can you please let us know.

what repo are you using? is the following?

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth

What toolchain are you using to compile? Did you installed metatoolchain?


Best regards,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信