flickering and splite when using imx8mn with icn6211 mipi to RGB convertor chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flickering and splite when using imx8mn with icn6211 mipi to RGB convertor chip

1,374 Views
AccuJie
Contributor III

Hi,

We have an imx8mn board with an icn6211 chip to convert the MIPI signal to an RGB signal. 

I port the driver which can show the image. However, sometimes the screen is flickering and split. I suspect it is the sync issue or with the DRM driver?

AccuJie_0-1641528763188.jpeg

 

I posted a demo video here https://www.youtube.com/watch?v=00nUH5keII8. The split and flickering are very weird since it seems related to the content of the image. And always have the same width between each splitting. 

Here is the datasheet from our LCD 800*480. 

AccuJie_0-1641317055567.png

 

Here is the parameters I make for the screen:

 

 

static const struct drm_display_mode jy20f56_mode = {
	.clock = 33300,
	.hdisplay = 800,
	.hsync_start = 800 + 210,
	.hsync_end = 800 + 210 + 10,
	.htotal = 800 + 210 + 10 + 36,
	.vdisplay = 480,
	.vsync_start = 480 + 22,
	.vsync_end = 480 + 22 + 8,
	.vtotal = 480 + 22 + 8 + 15,
};

static const struct panel_desc jy20f56 = {
	.modes = &y20f56_mode,
	.num_modes = 1,
	.bpc = 8,
	.size = {
		.width = 154,
		.height = 88,
	},
	.bus_format = MEDIA_BUS_FMT_RGB888_1X24,
};

 

 

 

Now I don't have any idea how to debug this kind of issue.

Really appreciate anyone who has any experience or idea.

 

Thanks,

Jie

 

 

0 Kudos
Reply
3 Replies

1,353 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?Can you try the newest BSP?

0 Kudos
Reply

1,349 Views
AccuJie
Contributor III

Hi, 

Thanks for your reply.

 

The BSP version I used is 5.4.24 zeus. Have you ever seen this kind of issue before?

Compiling of the latest BSP is really time consuming. I will have a try this week later.

0 Kudos
Reply

1,345 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can set drm debug mode to see more log when this issue happened.

0 Kudos
Reply