flexcan linux 3.8 : cannot find device "can0"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexcan linux 3.8 : cannot find device "can0"

Jump to solution
13,418 Views
gfritz
Contributor II

I use a i/MX286 processor and I would like to use the CAN controller inside. So I compiled my Linux 3.8 with CAN support (CAN, CAN RAW, Flexcan, etc...) in static. I have also updated the .dts to set the status to "okay" for the CAN0.

Linux boot correctly, but when I try to set up the can 0 with "ip link set can0 up type can bitrate 125000", linux tell me that it "cannot find device can0"

Did I forgot something ?

Thanks in advance

Gilles

PS: my bootloader is u-boot 2013.04

Labels (2)
0 Kudos
Reply
1 Solution
9,378 Views
x10
Contributor V

In my case of Linux-3.9.7, socket can does work with "/dev/can0".

View solution in original post

0 Kudos
Reply
6 Replies
9,378 Views
krishnanp
Contributor III

Hi, there

I am working on  i.MX6q sabre-lite board and trying to enable CAN bus  for the same. The CAN interface  configuration has been enabled in the dts file and Freescale Flexcan driver support enabled in Kernel. Looking at the dmesgs I am able to see the CAN driver init is happening. But  when I issue a ifconfig -a  which is not listing the CAN interface.

On the board dts file.

--------------------------------

&can1 {

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_flexcan1_1>;

        status = "okay";

};

On the processor dts file

-----------------------------------

                        can1: flexcan@02090000 {

                                compatible = "fsl,imx6q-flexcan";

                                reg = <0x02090000 0x4000>;

                                interrupts = <0 110 0x04>;

                                clocks = <&clks 108>, <&clks 109>;

                                clock-names = "ipg", "per";

                        };

                        can2: flexcan@02094000 {

                                compatible = "fsl,imx6q-flexcan";

                                reg = <0x02094000 0x4000>;

                                interrupts = <0 111 0x04>;

                                clocks = <&clks 110>, <&clks 111>;

                                clock-names = "ipg", "per";

                        };

I have debugged the CAN driver init on kernel boot log. The kernel log message  looks like below.

calling  can_init+0x0/0x108 @ 1

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

initcall can_init+0x0/0x108 returned 0 after 9945 usecs

calling  raw_module_init+0x0/0x40 @ 1

can: raw protocol (rev 20120528)

initcall raw_module_init+0x0/0x40 returned 0 after 2922 usecs

calling  bcm_module_init+0x0/0x70 @ 1

can: broadcast manager protocol (rev 20120528 t)

initcall bcm_module_init+0x0/0x70 returned 0 after 4290 usecs

calling  cgw_module_init+0x0/0x110 @ 1

can: netlink gateway (rev 20130117) max_hops=1

Looks like  i have to do some changes in my dts file. Any pointers on this?

Your help will be appreciated...

9,378 Views
krishnanp
Contributor III

This issue was rectified. It dis appeared when I recompiled the kernel and enabled Virtual can option.

0 Kudos
Reply
9,378 Views
gfritz
Contributor II

Hi,

thank for your help. After a little pause due to work, I managed to run correctly flexcan on linux 3.8 with xenomai. I don't know what's happend, I'd just rewrite the dts....

0 Kudos
Reply
9,379 Views
x10
Contributor V

In my case of Linux-3.9.7, socket can does work with "/dev/can0".

0 Kudos
Reply
9,378 Views
lategoodbye
Senior Contributor I

Hi Gilles,

please check first the Booting messages from Kernel for any CAN specific output and a existing CAN interface with:

ifconfig -a

0 Kudos
Reply
5,762 Views
Ingriid
Contributor II

Hi in my case, i tried with ifconfig -a, and i did not have any response grom kernel regarding Can.

what would be the possible problem?

I already installed canutils, modified the tree file, Also enabled "network utilities". Copy and create an imx image-multimedia image, and I keep getting the same problem.

0 Kudos
Reply